For a reliable and safe press-in process HARTING has developed a special
tooling system.
Each tooling is adapted to the special requirements of the individual connector
range, thus a good handling and quick adjustment is guaranteed.
The different demands of the system designs will be covered from the highly
adaptable tooling system for AdvancedTCA® or MicroTCA™ with the following
options:
Guiding of the connector and alignment of the top and the bottom tool
Guiding of the pcb and alignment of the top and the bottom tool